2013-05-17 12:48 AM
I looking for a download link of the STM32F10x DSP Library, there multiple references to it and a user manual (UM0585) but cannot find the actual code anywhere... Anyone?
2013-05-17 4:49 AM
It is at least explicitely available for ST's M4 cores, say, the F3 and the F4, where you can download it as STM32Fxxx_DSP_StdPeriphLib_Vxxx.
The DSP part is provided by ARM, and can be used/compiled for M0, M3 and M3 cores. Perhaps ST doesn't see DSP-like applications as a primary market for the F1xx series2013-05-20 2:34 AM
Well, I have inherited a project that uses the fore mentioned library but modified without explicit comments...The original lib is actually written by ST and is in assembly. I need to get my hands on the original lib so I can do a diff to evaluate the modifications that have been performed... I suppose it must have been moved to the legacy staff, but nevertheless I need access to it.
Anybody?2013-05-20 3:56 AM
It looks like I never installed it but the installer itself is still on my drive, file attached.
________________ Attachments : um0585.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0r7&d=%2Fa%2F0X0000000beW%2FlGmMORuX2BlUJRcE2BLkDhbyvetWUgfKAjYulaCMOn4&asPdf=false