2015-01-23 9:55 AM
Can some of the pins of a peripheral be remapped while others stay at their existing AF location? I noticed in reference code on the STM32F107 that appears that some of the pins are remapped, but not all of them.
I want to dynamically remap the SS pin for SPI3 to drive two devices, can this be done without moving the MISO, MOSI, and SCLK pins?2015-01-23 10:18 AM
What does the Reference Manual suggest?
Drive the Chip Select as a GPIO, then you can use any pin(s) you want.