STM32F107 I2C2 not clocking the SCL line.
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-07-10 9:16 AM
Is there an alternate function that needs to be disabled for this to work by default? The datasheet footnote says "SPI2/I2S2 and I2C2 are not available when the Ethernet is being used."
Is the Ethernet enabled by default and how do I disable it or properly configure the I2C2 port on pins PB10 and PB11?
Labels:
- Labels:
-
I2C
-
STM32F1 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0