cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F107 I2C2 not clocking the SCL line.

JMara.5
Associate II

Is there an alternate function that needs to be disabled for this to work by default? The datasheet footnote says "SPI2/I2S2 and I2C2 are not available when the Ethernet is being used."

Is the Ethernet enabled by default and how do I disable it or properly configure the I2C2 port on pins PB10 and PB11?

0 REPLIES 0