cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103Z USART strange output

samed
Associate II
Posted on November 12, 2013 at 16:38

Hello,

I'm using a SM3210e-Eval board with a

http://www.mikrocontroller.net/part/STM32F103

Z processor from

http://www.mikrocontroller.net/articles/ARM

and I'm a newbie . I dont really get why but if I send I getting a different value on my Terminal (hterm)

Example:

I'm sending 0x49 but get 8698 (Hex)

I'm sending 'A' but get FE06 (Hex)

I'm sending '0' but get F800 (Hex)

I'm not sure but do I need to change some clockspeed in the SystemInit() ?

But which one and how much ? I'm really lost....trying since 2 days solve this problem...

USART_InitTypeDef USART_InitStructure;

void

main(

void

) { SystemInit(); Init(); Config_ADC(); Config_Usart(); ...

while

(

1

) { USART_SendData(USART1,

0x49

);

//

/* Loop until the end of transmission */

while

(USART_GetFlagStatus(USART1, USART_FLAG_TC) == RESET) { } } }

void

Config_Usart() {

//enable bus clocks

RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1 | RCC_APB2Periph_GPIOA | RCC_APB2Periph_AFIO, ENABLE);

/* Configure USART2 Tx as alternate function push-pull */

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); USART_InitStructure.USART_BaudRate =

9600

; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

/* Configurating and enabling USART1 */

USART_Init(USART1, &USART_InitStructure); USART_Cmd(USART1, ENABLE); }

#stm3210e-eval #usart
This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
Posted on November 12, 2013 at 16:54

Sounds like a timing problem. Have you looked at the signal with a scope? Confirmed bit timing?

Most likely a project level disagreement between the define HSE_VALUE and the crystal on the board.

What tool chain? Normally SystemInit() is called prior to main() being called. You using CooCox?

What if you don't call SystemInit(), or  comment out it's body? This should run the board at 8 MHz from the HSI clock source. Does that work?
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
samed
Associate II
Posted on November 12, 2013 at 17:29

I'm using Keil as toolchain. And I already selected there my device SM32F103ZG.

You mean comment out in file system_stm32f10x.c ? Or just in my main() ?

Posted on November 12, 2013 at 18:30

If you're using the v3.5.0 CMSIS version of the firmware library, SystemInit() should have been called in startup_stm32f10x_xx.s, you should not be calling in again in main().

The quickest way to get the board to run from HSI would be to comment out the body code for SystemInit() in system_stm32f10x.c

ie

void SystemInit(void)

{

#if 0

// .. Body thereof

#endif

}

Check what value you have for HSE_VALUE within your project's pre-processor defines, or perhaps stm32f10x_conf.h

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
samed
Associate II
Posted on November 13, 2013 at 13:16

Hey commented out the SystemInit() body and it worked.!!!! THANKS !!!

That means the mistake was there ....

so next step ist to change the SystemInit ?

Or can I solve the problem in a other way ?

samed
Associate II
Posted on November 13, 2013 at 16:40

My preprocessor Symbols has defined STM32F10X_HD_VL

The SetSysClock() function in SystemInit is the problem

in the system_stm32f10x.c:

#if defined (STM32F10X_LD_VL) || (defined STM32F10X_MD_VL) || (defined STM32F10X_HD_VL)

/* #define SYSCLK_FREQ_HSE    HSE_VALUE */

 #define SYSCLK_FREQ_24MHz  24000000

#else

/* #define SYSCLK_FREQ_HSE    HSE_VALUE */

/* #define SYSCLK_FREQ_24MHz  24000000 */

/* #define SYSCLK_FREQ_36MHz  36000000 */

/* #define SYSCLK_FREQ_48MHz  48000000 */

/* #define SYSCLK_FREQ_56MHz  56000000 */

#define SYSCLK_FREQ_72MHz  72000000

#endif

.....

static void SetSysClock(void)

{

#ifdef SYSCLK_FREQ_HSE

  SetSysClockToHSE();

#elif defined SYSCLK_FREQ_24MHz

  SetSysClockTo24();

#elif defined SYSCLK_FREQ_36MHz

  SetSysClockTo36();

#elif defined SYSCLK_FREQ_48MHz

  SetSysClockTo48();

#elif defined SYSCLK_FREQ_56MHz

  SetSysClockTo56();  

#elif defined SYSCLK_FREQ_72MHz

  SetSysClockTo72();

#endif

 

 /* If none of the define above is enabled, the HSI is used as System clock

    source (default after reset) */

}

Posted on November 13, 2013 at 16:59

It is critical for you to understand the crystal on your board, and the value defined for HSE_VALUE within you project.

Suggest using your working HSI USART example, and printing out the value of HSE_VALUE the project is built with.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
samed
Associate II
Posted on November 13, 2013 at 17:21

my HSE_VALUE is 8000 000  i tried to make a preprocessor Symbol define in my Keil: HSE_VALUE=8000000

but it didnt worked...

I also run an ADC on my board , when the SystemInit() is comment everything slows down like my ADC but my USART works well.... Is there a way to solve this ?

Posted on November 13, 2013 at 17:37

Have you tried using some of the template projects for your board included in the firmware library, and USB examples?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..