cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103VBT6 USB not seen by PC

Posted on August 18, 2016 at 18:19

Please delete.

2 REPLIES 2
slimen
Senior
Posted on August 19, 2016 at 15:24

Hi,

'' I 

am using STM32F103RBT6. I am trying to power up the USB CDC project generated by CubeMx. This however doesnt work- Computer doesnt see the device at all. I remember I used to generate such project for an F4 device and it worked just fine. I was wondering either there is any additional code that has to be run in order to turn this module on? 

I am 100% sure that the physical connections are correct. USBDP is connected to PA12 and USBDM to PA11.

I would appreciate all help really, I thought this is going to work out of the box and I am short on time now. ''

I am interested to know how you fixed your issue.

Please avoid removing the content of the post describing your issue.

It will be more interesting to keep the description, then let us know how you resolved the case. It may be helpful for other forum users.

Regards
Posted on August 19, 2016 at 15:30

Hi,

The problem is I havent solved this. I made another topic explaining further what is going on:

[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32F1%20USB%20in%20CDC%20mode&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx&currentviews=0]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex%5fmx%5fstm32%2fSTM32F1%20USB%20in%20CDC%20mode&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https%3A%2F%2Fmy%2Est%2Ecom%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex%5Fmx%5Fstm32%2FAllItems%2Easpx&currentviews=0

I would still apreciate help regarding this issue.