cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32f103 Flash size

Akhil Francis
Associate II
Posted on August 30, 2017 at 13:06

Hi,

Actually i am using STM32F103VBT6, But now my code exceeds 128KB.

So with out changing my circuit can i use any of other Controllers of STM32F103 series which has more flash size and package should be LQFP100.

Fast reply will be helpful for me

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on August 30, 2017 at 13:19

Download the data sheet for the 256KB part and walking through the pin list, that should get you the answer fast.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
andy2399
Senior
Posted on August 30, 2017 at 14:43

I like to use SM32CubeMX for this.

  • Select the STM32F1 series.
  • Select LQFP100 in the package filter.
  • Adjust the flash size to 256K to 1024K

You will get a list of 15 matching items with easy access to each of their datasheets.

Andy