cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103CB ADC Interrupt based on timer does not trigger each pwm period?

eirik
Associate II
Posted on June 18, 2015 at 22:14

The original post was too long to process during our migration. Please click on the attachment to read the original post.
1 REPLY 1
Amel NASRI
ST Employee
Posted on June 22, 2015 at 11:44

Hi Eirik,

You can set the configuration you are expecting based on STM32CubeMX tool and generate the code allowing you to choose the timer as trigger for the ADC.

Then you will have to add the calls for data processing functions.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.