2017-01-29 12:04 PM
Hello All
i have a timer which runs at 10 khz and a adc channel in inject mode, the problem is i have set some gpio toggling inside the ADC1_2_IRQHandler, but nothing happens....
I cant explain why the ADC1_2_IRQHandler is not being triggerd...
This is my adc init code , i am using stm32f10x_md.s file, but i see its defined the irq for adc as
DCD ADC1_2_IRQHandler ; ADC1 & ADC2
and in my project setings i have defined STM32F10X_MD which coresponds in the stm32f10x.h file with bellow
#ifdef STM32F10X_MD
ADC1_2_IRQn = 18, /*!< ADC1 and ADC2 global Interrupt */NVIC_InitTypeDef NVIC_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure; ADC_InitTypeDef ADC_InitStructure; DMA_InitTypeDef DMA_InitStructure; NVIC_InitStructure.NVIC_IRQChannel = ADC1_2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority =4 ; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 4; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_4 ; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN; GPIO_Init(GPIOA, &GPIO_InitStructure); RCC_ADCCLKConfig(RCC_PCLK2_Div6); // ADC clock set to 72/6 = 12 MHZ RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 |GPIO_Pin_11|GPIO_Pin_12; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(GPIOB, &GPIO_InitStructure); /* DMA1 channel1 configuration ----------------------------------------------*/ DMA_DeInit(DMA1_Channel1); DMA_InitStructure.DMA_PeripheralBaseAddr = ADC1_DR_Address; DMA_InitStructure.DMA_MemoryBaseAddr = (u32)&(myadcz[0]); // Data direction: Peripheral is source DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC; DMA_InitStructure.DMA_BufferSize = 8; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; DMA_Init(DMA1_Channel1, &DMA_InitStructure); DMA_ITConfig(DMA1_Channel1, DMA_IT_TC, ENABLE); DMA_Cmd(DMA1_Channel1, ENABLE); /* Put everything back to power-on defaults */ ADC_DeInit(ADC1); /* ADC1 configuration ------------------------------------------------------*/ ADC_InitStructure.ADC_Mode = ADC_Mode_Independent; ADC_InitStructure.ADC_ScanConvMode = ENABLE; ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfChannel = 1; ADC_Init(ADC1, &ADC_InitStructure); ADC_RegularChannelConfig(ADC1, ADC_Channel_5, 1, ADC_SampleTime_71Cycles5); //PA5 - Analog channel 5 /* Enable ADC1 DMA */ //ADC_DMACmd(ADC1, ENABLE); // INJECTED /* Set injected sequencer length */ ADC_InjectedSequencerLengthConfig(ADC1, 1); /* ADC1 injected channel Configuration */ ADC_InjectedChannelConfig(ADC1, ADC_Channel_4, 1, ADC_SampleTime_71Cycles5); //PA4 - Analog ADC1 - channel 4 /* ADC1 injected external trigger configuration */ ADC_ExternalTrigInjectedConvConfig(ADC1, ADC_ExternalTrigInjecConv_T1_TRGO); ADC_ExternalTrigInjectedConvCmd(ADC1, ENABLE); /* Enable JEOC interrupt */ ADC_ITConfig(ADC1, ADC_IT_JEOC, ENABLE); /* Enable ADC1 */ ADC_Cmd(ADC1, ENABLE); /* Enable ADC1 reset calibaration register */ ADC_ResetCalibration(ADC1); /* Check the end of ADC1 reset calibration register */ while(ADC_GetResetCalibrationStatus(ADC1)); /* Start ADC1 calibaration */ ADC_StartCalibration(ADC1); /* Check the end of ADC1 calibration */ while(ADC_GetCalibrationStatus(ADC1)); /* Start ADC1 Software Conversion */ ADC_SoftwareStartConvCmd(ADC1, ENABLE);and my interrupt handler
void ADC1_2_IRQHandler(void){ GPIO_SetBits(GPIOB,GPIO_Pin_11);voltage = ADC_GetInjectedConversionValue(ADC1, ADC_InjectedChannel_1);
/* Clear ADC1 JEOC pending interrupt bit */
ADC_ClearITPendingBit(ADC1, ADC_IT_JEOC);GPIO_ResetBits(GPIOB,GPIO_Pin_11);}
2017-01-29 12:52 PM
are you using C++ ?
Can you put a break point in your code ?
I guess that ' void ADC1_2_IRQHandler(void)'
is not actually mapped into the linker.
can you find the original 'void ADC1_2_IRQHandler(void)' and put a break point in there too.
then you will know which one is being called.
if that is the problem then this could be your issue:
code needed to force linker to see your function.
extern 'C' void ADC1_2_IRQHandler(void){
.
.
.
}
2017-01-29 7:48 PM
Do you handle/see the DMA interrupt?
2017-01-29 11:25 PM