cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103 USB EXAMPLE

stefanofante9
Associate II
Posted on June 09, 2010 at 18:20

STM32F103 USB EXAMPLE

2 REPLIES 2
chikos332
Associate II
Posted on May 17, 2011 at 13:54

Hi,

are you using the version v3.1.1 of the USB library ? (I think that the isochronous IN is supported only in this version... there was a post about this issue in the past, try to find it).

Cheers.

stefanofante9
Associate II
Posted on May 17, 2011 at 13:54

Hi,

yes I'm using the last version of the libraries 3.1.1

I'm trying to port an application that I wrote for STR912

I didn't find any example for an IN transfer using ISOCHRONOUS EP

I'm able to configure and transfer data using BULK but when I try to select the EP as ISOCHRONOUS no EP irq are generated :-( !

There is a bug in the libs?