2010-06-09 09:20 AM
STM32F103 USB EXAMPLE
2011-05-17 04:54 AM
Hi,
are you using the version v3.1.1 of the USB library ? (I think that the isochronous IN is supported only in this version... there was a post about this issue in the past, try to find it). Cheers.2011-05-17 04:54 AM
Hi,
yes I'm using the last version of the libraries 3.1.1 I'm trying to port an application that I wrote for STR912 I didn't find any example for an IN transfer using ISOCHRONOUS EP I'm able to configure and transfer data using BULK but when I try to select the EP as ISOCHRONOUS no EP irq are generated :-( ! There is a bug in the libs?