Posted on May 17, 2011 at 14:23 Hi, try to add a pull-up resistance (~50KOhm) on the device TX line it should work. try it on your own risk, and be careful not to cause a short-circuit. Cheers.
Posted on May 17, 2011 at 14:23 Hi Sebastian, Are you interested of having a command line option for programming through USART (RS232 serial interface)? This option exists in ST Flash loader demonstrator tool. For the DFUse, you have to know that yo...
Posted on May 17, 2011 at 14:03 Hi, - If you are using the STM32F1x5xxx or STM32F1x7xxx devices, no chance, you can't use both USB and CAN (they have shared RAM). - For the IN endpoints, the Host is always sending IN requests to the device with fixe...
Posted on May 17, 2011 at 14:01 .ExternalClassC4E2F1C9E533482AA7F0BC43077A9412 p.MsoNormal, .ExternalClassC4E2F1C9E533482AA7F0BC43077A9412 li.MsoNormal, .ExternalClassC4E2F1C9E533482AA7F0BC43077A9412 div.MsoNormal {margin:0in;margin-bottom:.0001pt...
Posted on May 17, 2011 at 14:01Hi, The erase value for the flash is 0xFF. If you write any other value then try to write again, you will have either programming error or the value will not be correctly written. And as far as I know, the erase can be...