2024-10-11 01:41 PM
Hi, I am a beginner user of the stm32 board.
I am working with an ICM20607 IMU sensor, and I want to read the accelerometer data (x, y, z axes) using the Cube IDE.
I ve read a lot of sources for one week but couldn't find a way to fix it. I can't see something on my serial port. What am I missing? Thank you.
Here is the code and pins:
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* Copyright (c) 2024 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include "stm32f1xx_hal.h"
#define ICM20607_ADDRESS 0x68 << 1 // I2C address of ICM20607
#define ACCEL_XOUT_H 0x3B
#define ACCEL_XOUT_L 0x3C
#define ACCEL_YOUT_H 0x3D
#define ACCEL_YOUT_L 0x3E
#define ACCEL_ZOUT_H 0x3F
#define ACCEL_ZOUT_L 0x40
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
I2C_HandleTypeDef hi2c1;
UART_HandleTypeDef huart2;
/* USER CODE BEGIN PV */
uint16_t Data = 0;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C1_Init(void);
static void MX_USART2_UART_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
void icm20607_init(void) {
uint8_t reset_cmd = 0x80; // Reset command
HAL_I2C_Mem_Write(&hi2c1, ICM20607_ADDRESS, 0x6B, 1, &reset_cmd, 1, HAL_MAX_DELAY);
HAL_Delay(100); // Wait for reset
uint8_t config = 0x01; // Gyro and Accel on
HAL_I2C_Mem_Write(&hi2c1, ICM20607_ADDRESS, 0x6B, 1, &config, 1, HAL_MAX_DELAY);
}
void read_acceleration(int16_t *ax, int16_t *ay, int16_t *az) {
uint8_t buffer[6]; // Buffer for accelerometer data
HAL_I2C_Mem_Read(&hi2c1, ICM20607_ADDRESS, ACCEL_XOUT_H, 1, buffer, 6, HAL_MAX_DELAY);
// Combine high and low bytes
*ax = (int16_t)((buffer[0] << 8) | buffer[1]);
*ay = (int16_t)((buffer[2] << 8) | buffer[3]);
*az = (int16_t)((buffer[4] << 8) | buffer[5]);
}
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_I2C1_Init();
MX_USART2_UART_Init();
icm20607_init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
int16_t ax, ay, az;
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
read_acceleration(&ax, &ay, &az);
// Prepare string to send via UART
char msg[100];
snprintf(msg, sizeof(msg), "accX: %d, accY: %d, accZ: %d\r\n", ax, ay, az);
HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
HAL_Delay(100); // Delay for readability
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL9;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief I2C1 Initialization Function
* @PAram None
* @retval None
*/
static void MX_I2C1_Init(void)
{
/* USER CODE BEGIN I2C1_Init 0 */
/* USER CODE END I2C1_Init 0 */
/* USER CODE BEGIN I2C1_Init 1 */
/* USER CODE END I2C1_Init 1 */
hi2c1.Instance = I2C1;
hi2c1.Init.ClockSpeed = 400000;
hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
hi2c1.Init.OwnAddress1 = 0;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN I2C1_Init 2 */
/* USER CODE END I2C1_Init 2 */
}
/**
* @brief USART2 Initialization Function
* @PAram None
* @retval None
*/
static void MX_USART2_UART_Init(void)
{
/* USER CODE BEGIN USART2_Init 0 */
/* USER CODE END USART2_Init 0 */
/* USER CODE BEGIN USART2_Init 1 */
/* USER CODE END USART2_Init 1 */
huart2.Instance = USART2;
huart2.Init.BaudRate = 115200;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART2_Init 2 */
/* USER CODE END USART2_Init 2 */
}
/**
* @brief GPIO Initialization Function
* @PAram None
* @retval None
*/
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @PAram file: pointer to the source file name
* @PAram line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
2024-10-11 01:47 PM
Here you can find help with any aspect of your STM32 project. Software, electronics and more.
2024-10-11 04:13 PM
>>I ve read a lot of sources for one week but couldn't find a way to fix it.
Ok, but what DOES happen?
Do the I2C functions read anything? Do they return error or status codes?
Can you read any of the STATUS or WHOAMI registers?
How's this wired? You have external pull-ups?
You have this sensor on a board? You've looked at the signals with an oscilloscope or logic analyzer?
2024-10-11 05:14 PM
I'm here to learn, not copy-paste someone's code. Sorry, you're only making an advertisement here.
2024-10-11 05:20 PM - edited 2024-10-13 07:48 PM
yes, this imu sensor is on the board. I don't have any wiring on board. Do I need it? Do I need to check signals? the board is new, and I run another code on it without issue.
there is no warning or error for the code.
I only see these. , ax - ay- az
2024-10-12 10:50 AM
Hi,
With all respect, not only an advertisement. Rather, an life buoy. Imagine you're driving somewhere and run out of gas. You tell a stranger that you need gas. He says "here's a gas station around the corner" . "No! you're advertising" you reply.
2024-10-13 11:21 AM
@stmuser3535 wrote:yes, this imu sensor is on the board. I don't have any wiring on board. Do I need it? Do I need to check signals? the board is new, and I run another code on it without issue.
there is no warning or error for the code.
I only see these. , ax - ay- az
So you have data and you're trying to send over huart2. So how is UART2 connected to the outside world? What are you using to view this data? Baud rate match both ends?
2024-10-13 07:48 PM
The data should come from the integrated IMU sensor as x,y, and z. For example, generally, we can use mpu6050 for those cases. I am using console view > serial port in CubeIde. @Karl Yamashita
2024-10-14 12:25 AM
Again, you've shown you have data. I'm trying to see your issue with
I can't see something on my serial port.
So how are you connecting the UART2 to the outside world, in this case the STM32CubeIDE console?
2024-10-14 09:24 AM - edited 2024-10-14 09:25 AM
UART2 is routed through the st-link interface to the usb port. Am I correct? @Karl Yamashita
baud rate 115200