cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103 - DAC

jaykov
Associate II
Posted on August 02, 2015 at 14:00

Hi dear friends,

I have the SMT32F103RCT6 and I trying to use the DAC with DMA. I compile the ''OneChannelDMA_Escalator'' example and unfortunately it won't work, When I change the code so it will work without the DMA i can see the signal in my scope.

I attach the code that i using,

Regards, Yakov S.

#dac #gpio #dma #stm32f103
This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
raptorhal2
Lead
Posted on August 04, 2015 at 23:21

I don't see any DMA/TIM errors, and don't have a HD F103 to try the code. Perhaps someone else can spot something.

Cheers, Hal