2009-02-01 06:37 PM
STM32F101x4 IAR version
2011-05-17 04:01 AM
Hello, Can anyone notify me if the IAR EWARM-KS-WEB-5301.EXE is suitable for the low density micro STM32F101x4? I was using the IAR version that comes with development board STM32-SK, and the program was halting during download. Im suspecting that this IAR version is not suitable for STM32 low density micros. Thanks Johann
2011-05-17 04:01 AM
Yes the new version 5.30 is suitable with the low denstity devices:
http://www.iar.com/website1/1.0.1.0/94/1/index.php?2011-05-17 04:01 AM
This is is the same one I downloaded. Can anyone help me how to set it to work on STM32F101C4. I'm sending the error message I'm obtaining in a doc file. Thanks Johann
2011-05-17 04:01 AM
just select ''ST STM32F10xx4'' as device name in options->target->Device
and check that the flash loader is set to default.2011-05-17 04:01 AM
Hello jilisegiar. Thanks for your reply. Can you please indicate to me the file that I need to download? Many thanks Johann I downloaded 5.4 and is not working on the low end micro. Thanks Johann
2011-05-17 04:01 AM
Hello jilisegiar, Thanks very much it worked. Johann