Posted on May 17, 2011 at 13:24Hi All. Please does any one have a circuit to use the L656x in non-isolated buck controller. The application notes, are all on the isolated power supply. I need it to provide power for the STM32 micro from AC source. I...
Posted on May 17, 2011 at 13:12Hello Many thanks. the problem seems to have been related to the pull down resistor I was using with BOOT0. This was 47k. When I lowered it down to 4k7, it was working well. thanks Johann
Posted on May 17, 2011 at 13:12Hello, I'm using the micro STM32F101C4 and occasionally when I turn ON the micro, the program seems that it does not start. Right now I'm using TIM3 to blink LED and occasionally it does not turn ON. I have to turn OFF...