cancel
Showing results for 
Search instead for 
Did you mean: 

USB OTG on STM32

stm322
Associate II
Posted on January 30, 2009 at 14:47

USB OTG on STM32

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
stm322
Associate II
Posted on May 17, 2011 at 13:01

Hello,

I'm trying to do the following thing:

a STM32 working as USB virtual com port. For that ST provide VCP example.

And on the other side, instead to plug a PC to recognise this VCP, I would like to plug another STM32.

Apparently, this second STM32 needs to have USB OTG.

Does anyone know if ST provides a USB OTG library for STM32?

Thanks in advance.

sword_82
Associate II
Posted on May 17, 2011 at 13:01

Hello stm321,

STM32 doesn't support USB OTG, it provides the device capability only. In other words, the STM32 cannot be a host it can be only a device!

regards

sword

stm322
Associate II
Posted on May 17, 2011 at 13:01

ok.

Thank you very much.

st3
Associate II
Posted on May 17, 2011 at 13:01

To connect two STM32s together, just using the UARTs would be far simpler. 8-)