cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F100RBT6. I left HAL libraries behind and want to work writing straight to the registers but something is wrong and it does not work.

FAleg.1
Associate II

I want to blink a LED and I have written this code:

#include "stm32f10x.h"

int main()

{

// initialize the clock for Port C

RCC->APB2ENR |= (1<<4); // enable clock for GPIO C ( check it on memory and bus architecture)

// set pin 9 of GPIOC to output mode

GPIOC->CRH |= ((1<<4)|(1<<5)); // PC9 pin will be used as an Output at max speed = 50 MHz

GPIOC->CRH &= (unsigned int)~((1<<6)|(1<<7)); // output mode in push-pull configuration (set 11 to CNF bits), that is, General Purpose Output

int i;

while(1)

{

for(i=0;i<=5000000;i++);

GPIOC->BSRR = (1<<9);

for(i=0;i<=5000000;i++);

GPIOC->BSRR = (1<<(9+16));

}

}

// keil requires you to leave an extra line after the last bracket

The output for PC9 only yields a weird 5MHz pulse for any possible value I write in the comparison for loop field. At last, the LED turns on but as I'm using 8MHz for system clock, it should blink at a rate I would be able to see (i<=5000000 gives a 625ms switching period).

So, am I missing any register setting or whatnot?

Thank you in advance.

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
waclawek.jan
Super User

Qualify i as volatile.

Decrease the constant, roughly 10x.

Single-step in disasm both versions to see the difference.

>using 8MHz for system clock

Are you sure?

JW

Hi JW, it worked. I qualified i as volatile and reduced the constant, but why did that work? I have seen other people doing exactly like that (but using STM32F103C8T6) and it did work.

Yet I still do not understand 2 other situations:

why can I not watch the variable while debugging (<cannot evaluate> for both int or volatile int types) ?

and why is it not 8 MHz for system frequency?

Piranha
Chief II

https://blog.regehr.org/archives/28

Without volatile your loop is doing nothing useful and compiler is not required to keep it. That happens when some optimization is turned on and that is also the reason you cannot watch some variables.

KnarfB
Super User

Just a remark: there are predefined constants which make your code more readable like (for a different chip):

	RCC->AHBENR |= RCC_AHBENR_GPIOBEN;	// GPIO port B clock enable
 
	GPIOB->MODER   |=  GPIO_MODER_MODER3_0; 	// mode 01: GPIO output
	GPIOB->MODER   &= ~GPIO_MODER_MODER3_1; 	// mode 01: GPIO output
	GPIOB->OTYPER  &= ~GPIO_OTYPER_OT_3; 		// type: push-pull
	GPIOB->OSPEEDR &= ~GPIO_OSPEEDER_OSPEEDR3;	// speed 00: low speed
	GPIOB->PUPDR   &= ~GPIO_PUPDR_PUPDR3;		// no pull-up, no pull-down
 
	for(;;) {
		GPIOB->BSRR = GPIO_BSRR_BS_3;			// Bit Set
		delay();
		GPIOB->BSRR = GPIO_BSRR_BR_3;			// Bit Reset
		delay();
	}

waclawek.jan
Super User

> and why is it not 8 MHz for system frequency?

Some code in startup (SystemInit() or similar) which changes the RCC settings?

JW

TDK
Super User

I suggest implementing a version of HAL_Delay that works if you need a delay functionality.

If you feel a post has answered your question, please click "Accept as Solution".