cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F100RB wifi

teo yalun
Associate
Posted on March 11, 2018 at 14:51

hi, can i use STM32F100RB to interface SPWF04SA via UART or SPI? i checked around no much example using these two together. any API or tutorial example i can use and follow?

2 REPLIES 2
Posted on March 11, 2018 at 15:22

You perhaps want to look at the Nucleo shield board, and software

http://www.st.com/en/ecosystems/x-nucleo-idw04a1.html

 

http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-expansion-packages/x-cube-wifi1.html

 

and port functionality back from the NUCLEO-F103RB examples

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
henry.dick
Senior II
Posted on March 11, 2018 at 15:27

'

can i use STM32F100RB to interface SPWF04SA via UART or SPI?'

yes, if you can get both to talk the same protocol.