2017-04-05 07:19 AM
I want to know how TIM2 of STM32F100 works. Can someone help me?
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;uint16_t PrescalerValue = 0;RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;TIM_TimeBaseStructure.TIM_Prescaler = (uint16_t) (SystemCoreClock / 1000) - 1;TIM_TimeBaseStructure.TIM_Period = 999;I don't understand why TIM_Period is 999.
2017-04-05 07:34 AM
The counter goes through 0 to N-1, this has N states. The logic for comparing if the current count is N-1, and resetting/updating at the next clock is simpler to implement.
OutClock = TIMCLK / (P * Q); where Prescaler = Q-1, and Period = P-1
Your example looks to generate a 1Hz update. It prescales the TIMCLK to 1 KHz, and then counts off 1000 ticks.
2017-04-05 07:34 AM
Hi
toader.alexandra
,I'd highly recommend you to refer to TIM example under the
firmware package. The example is found under the path below: STM32Cube_FW_F1_V1.4.0\Projects\STM32VL-Discovery\Examples\TIM\TIM_TimeBaseThe example titled 'TIM_TimeBase' shows how to configure the TIM peripheral to generate a time base of one second with the corresponding Interrupt request.
You may take this example as a reference to correctly configure your peripheral.Khouloud
2017-04-05 09:46 AM
Thanks,
so who is P and Q?
2017-04-05 09:46 AM
OP is using the SPL, and doesn't understand the timer/counter at a conceptual level. ie the mechanics of the timer, and why the values are chosen
2017-04-05 10:36 AM
They would be factors.
If you know what frequency you want to generate, you have to determine what two integer divisors are required to get there from the input clock, assuming in this case both must fit in 16-bit, so can't exceed 65536
The TIM is clocked via the APB bus, if that's 24 MHz, dividing it by 24000 gets you to 1 KHz, ie a prescaler of 24000-1 or 23999
To get an update period of 1 Hz you must divide the 1 KHz by 1000,ie a period of 1000-1 or 999
So if TIMCLK = 24000000, and Q=24000 and P=1000
OutClock = 24,000,000 / (24000 * 1000)
OutClock = 1 Hz
2017-04-05 11:19 AM
sorry but i don't understand why you divide the 24 MHz by 24000? Why 24000? From where you get 24000?
2017-04-05 12:54 PM
It comes from (SystemCoreClock / 1000)
Where SystemCoreClock is 24,000,000 (what you're running the processor and buses at)
Divided by 1000, gets us 24000 (a valid integer between 1 and 65536)
24,000 ticks of a 24 MHz clock source takes 1ms, and 1ms is 1KHz
After the prescaler the TIM count increments every 1ms, a thousand of those and you've got yourself a second.
The equation for the TIM Update, ie when it rolls back to zero (0..999)
OutClock = (24,000,000 / 24,000) / 1,000
2017-04-05 03:50 PM
thank you so much
2017-04-05 07:10 PM