cancel
Showing results for 
Search instead for 
Did you mean: 

Error for foc sdk v3.2

julienboudens9
Associate II
Posted on March 28, 2013 at 16:48

Error for foc sdk v3.2

Hello,

I compile the library foc sdk v3.2 with Atollic for stm32f100b and with gnu I have always the same error :

C:\VSS\MC\3PH\012\SOFTWARE\FIRMWARE\MC SDK v3.3\MC library\src\MotorPowerMeasurementClass.c:(.text+0x34): undefined reference to `__aeabi_memclr'

Do you have an idea for this error ? Thank you,
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Gigi
ST Employee
Posted on March 29, 2013 at 09:11

Ciao Julien,

I thnik that you are triyng to mix to much! I read v3.2 one line and v3.3 in the next.

Moreover the WEB distribution has been released with the compiled part compatible just with IAR so if you want to do the porting on Atollic is necessary that you start from the sources.

If you request is justified with a businnes you can try to get the source code contacting your nearest ST office.

Ciao

Gigi

Laurent Ca...
Lead II

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards