STM32F1 - LL_GPIO_Init() problem
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-17 12:45 PM
Hi,
A piece of code from STM32CubeMX v4.0 and latest F1 drivers generated for STM32VLDiscovery (the button is pulled-down by external resistor):
static void MX_GPIO_Init(void)
{LL_GPIO_InitTypeDef GPIO_InitStruct;
/* GPIO Ports Clock Enable */
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_GPIOC); LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_GPIOD); LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_GPIOA);GPIO_InitStruct.Pin = LL_GPIO_PIN_0;
GPIO_InitStruct.Mode = LL_GPIO_MODE_FLOATING; LL_GPIO_Init(GPIOA, &GPIO_InitStruct);}
and the results from the Keil debugger:
So commented the line below to prove that there is only one line of code used for GPIOA initialization:
// LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
and got as expected (the default settings for GPIOA)
It seems that the LL_GPIO_Init gives messy config on more than one pin. Am I wrong?
Have no luck with F1 line and LL drivers - this issue seems to be continuation of my previous finding:
--------------------------------
So switching back to register programming when working with boards with low SRAM size. It takes less time than investigating issues in LL drivers.
I wonder if you use LL drivers for F1 line. I know that more people prefer SPL drivers for this line.
Note: this post was migrated and contained many threaded conversations, some content may be missing.Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-18 3:25 AM
Getting more confused, I found this in the LL documentation
void LL_GPIO_StructInit (LL_GPIO_InitTypeDef * GPIO_InitStruct)
Set each LL_GPIO_InitTypeDef field to default value.So I changed my code to this:
LL_GPIO_StructInit(GPIOA);
GPIO_InitStruct.Pin = LL_GPIO_PIN_4|LL_GPIO_PIN_5;
GPIO_InitStruct.Mode = LL_GPIO_MODE_FLOATING;LL_GPIO_Init(GPIOA, &GPIO_InitStruct);GPIO_InitStruct.Pin = LL_GPIO_PIN_3|LL_GPIO_PIN_6|LL_GPIO_PIN_7;
GPIO_InitStruct.Mode = LL_GPIO_MODE_OUTPUT;GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH;GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;LL_GPIO_Init(GPIOA, &GPIO_InitStruct);As expected, before the LL_GPIO_StructInit(GPIOA) the settings of GPIOA looked like this
To my surprise the LL_GPIO_StructInit(GPIOA) did this to the actual settings of GPIOA
I didn't expect any change at all, I thought it would only fill the structure with the defaults, not actually changing anything in the uC. No doubt I (a hobbyist too) am doing things wrong but for me the docs are quite confusing.
And in the end it didn't help, GPIO_PIN_5 still got changed from input to output. The only thing that seems to help is configuring every GPIO_PIN separately.
EDIT: I'm starting to understand why it changes the actual GPIOA, but not with the values of it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-18 4:07 AM
Not
LL_GPIO_StructInit(GPIOA);
but
LL_GPIO_StructInit(&GPIO_InitStruct);
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-18 4:10 AM
Ah, that makes sense!
Still learning :)
Unfortunately it doesn't help preventing
GPIO_InitStruct.Pin = LL_GPIO_PIN_3|LL_GPIO_PIN_6|LL_GPIO_PIN_7;
GPIO_InitStruct.Mode = LL_GPIO_MODE_OUTPUT;GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH;GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;LL_GPIO_Init(GPIOA, &GPIO_InitStruct);from changing the settings for LL_GPIO_PIN_5
I'm also considering going back to register-programming. And I think that is a shame as reading the above lines is more explanatory than lines like this:
GPIOA->CRL &= ~GPIO_CRL_MODE0;
GPIOA->CRL |= GPIO_CRL_CNF0_0;GPIOA->CRL |= GPIO_CRL_MODE1;
GPIOA->CRL &= ~GPIO_CRL_CNF1;GPIOA->CRL |= GPIO_CRL_MODE2;
GPIOA->CRL &= ~GPIO_CRL_CNF2_0;GPIOA->CRL |= GPIO_CRL_CNF2_1;- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-19 12:39 AM
I mostly generate HAL skeleton for a project but in this case due to limited SRAM memory I wanted to use LL.
I used to use LL drivers for L0 boards ( I guess) and do not remember such basic problems with GPIO.
Going back to registers is good to re-fresh what is going on under the hood;)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-19 4:16 AM
'
Going back to registers is good to re-fresh what is going on under the hood;)'
in the end, going to registers may take you less time than necessary to understand and debug LL.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-19 5:57 AM
True, but for me there is the advantage of learning.
I'm a hobbyist who long ago programmed in assembler on the 6502, later also in asm on the atmel tiny and mega chips. Years later I switched to programming in C and only recently took the jump to STM
I started using the SPL but then I was told that that was a dead end (like now starting with python2) and that the Cube/HAL was the way forward.
But I do not like what it produces, eg the way interrupts are handled with callbacks. So LL it was, as it 'looks' better than register programming.
I am a hobbyist, I don't care how long something takes to get working, I don't get payed for it anyway. When something doesn't work as expected I love the search for why. Usually I'm the cause. Sometimes Im not. And I learn in both cases. So thanks for all the help from the pro's here.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-19 7:58 AM
Dear all,
Thank you for the comments and opening the discussion on this GPIO LL driver limitation. Indeed, we confirm the issue , and we confirm it is fixed in STM32CubeF1 Firmware patch Package V1.6.1 which will be in a couple of days on public web site and available in CubeMx to download as well.
Cheers,
STOne-32
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-19 9:21 AM
Thank you for letting us know!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-19 10:07 AM
Just tested STM32CubeF1 Firmware patch Package V1.6.1 - GPIO works fine.
Thanks,

- « Previous
-
- 1
- 2
- Next »