cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F072 uart RX

Bs.1
Associate II

I am using UART4 from STM32F072VB with 9600 baudrate on inetrrupt basis.

uint8_t p[2] = {0,0}; // array to store data received on uart temporary

storing uart receive data in this array according to my program requirement.

uint8_t led_ip_cmd[5][16];//array to store

I want to see the real time values for led_ip_cmd[][] array......

I am trying to use watchpoint during debugging but unable to see the values....

how can i observe it in real time application...

main()

{

while (1)

 {

 for(uint32_t b=0; b<0x04; b++);  //initial delay

 HAL_UART_Receive_IT(&huart4, (uint8_t *)p, 2);  

 for(uint32_t b=0; b<0x02; b++);

}

}

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Pavel A.
Super User