cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f051c8t6 NVIC and USART Problem

lernd
Associate II
Posted on September 23, 2013 at 11:33

Hi,

I configured USART1 in stm32f051c8t6 but when i run the code on my h/w it goes hang. I dont  where it is hanging. whether because of  NVIC OR USART. But according to me it hang in NVIC because everything run ok..........

 Please help me resolve this issues.....

I have given my configuration bellow;;

 RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE) ;

 RCC_USARTCLKConfig(RCC_USART1CLK_SYSCLK);

    GPIO_InitStructure.GPIO_Pin = UART_TX_PIN ;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

    GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_2;

    GPIO_Init(UART_TX_PORT, &GPIO_InitStructure);

    GPIO_InitStructure.GPIO_Pin =  UART_DTR_PIN;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

    GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_2;

    GPIO_Init(UART_DTR_PORT, &GPIO_InitStructure);

    GPIO_InitStructure.GPIO_Pin = UART_RX_PIN ;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;

    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

    GPIO_Init(UART_RX_PORT, &GPIO_InitStructure);

  

    NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);

    USART_DeInit(USART1);

    USART_InitStructure.USART_BaudRate = 9600;

    USART_InitStructure.USART_WordLength = USART_WordLength_8b;

    USART_InitStructure.USART_StopBits = USART_StopBits_1;

    USART_InitStructure.USART_Parity = USART_Parity_No;

    USART_InitStructure.USART_Mode = USART_Mode_Tx | USART_Mode_Rx;

    USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

    USART_Init(USART1, &USART_InitStructure);

     

  // USART_ITConfig(USART1, USART_IT_TXE, DISABLE);

    USART_ITConfig(USART1, USART_IT_TC, ENABLE);

   USART_ITConfig(USART1, USART_IT_RXNE, ENABLE);

    USART_Cmd(USART1, ENABLE); 

/////////////////UART1 IRQ handler??????????????????????

void USART1_IRQHandler(void)

{

    if(USART_GetITStatus(USART1, USART_IT_RXNE)!= RESET)

        {

            USART_ClearITPendingBit(USART1, USART_IT_RXNE);

        }

   

    if(USART_GetITStatus(USART1, USART_IT_TC)!= RESET)

        {

            USART_ClearITPendingBit(USART1, USART_IT_TC);

        

            send_ctr++;

            if(send_ctr <= 13)

                {

                    uart_send_data = uart_msg[send_ctr];

                    USART_SendData(USART1, uart_send_data);

                    

                }

            else

                send_ctr = 0;

        }

    

}

#provide-complete-code #stm32f051c8t6-usart-hanging-prob
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on September 23, 2013 at 13:40

Needs RX configured as AF, please refer to other examples

You have an RXNE interrupt but really don't service the USART by reading it's data register.

You use the TC interrupt when TXE would be better.

It's not clear how your code ever sends the first element of the array, or if it ever stops sending data.

Likely gets stuck in interrupt state because RXNE not cleared.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
lernd
Associate II
Posted on September 24, 2013 at 13:49