2017-12-25 1:04 PM
Hi Guys
I'm trying to implement the function HAL_RTCEx_SetWakeUpTimer_IT in stm32f0xx_hal_rtc_ex.h file.
My device is STM32F031x6
However I see the following code in the .h file:
#if defined(STM32F071xB) || defined(STM32F072xB) || defined(STM32F078xx) || defined(STM32F091xC) || defined(STM32F098xx) || defined(STM32F070xB) || defined(STM32F030xC)
/* RTC Wake-up functions ******************************************************//** @defgroup RTCEx_Exported_Functions_Group2 Extended RTC Wake-up functions * @{ */ HAL_StatusTypeDef HAL_RTCEx_SetWakeUpTimer(RTC_HandleTypeDef *hrtc, uint32_t WakeUpCounter, uint32_t WakeUpClock);HAL_StatusTypeDef HAL_RTCEx_SetWakeUpTimer_IT(RTC_HandleTypeDef *hrtc, uint32_t WakeUpCounter, uint32_t WakeUpClock);uint32_t HAL_RTCEx_DeactivateWakeUpTimer(RTC_HandleTypeDef *hrtc);uint32_t HAL_RTCEx_GetWakeUpTimer(RTC_HandleTypeDef *hrtc);void HAL_RTCEx_WakeUpTimerIRQHandler(RTC_HandleTypeDef *hrtc);void HAL_RTCEx_WakeUpTimerEventCallback(RTC_HandleTypeDef *hrtc);HAL_StatusTypeDef HAL_RTCEx_PollForWakeUpTimerEvent(RTC_HandleTypeDef *hrtc, uint32_t Timeout);#endifDoes this mean that MCU's other than the list in the #if do not support rtc wakeup timers? surely not?
Many thanks:)
Xarion2018-01-09 10:39 AM
2018-01-18 1:59 PM
I have exactly same question with you, do you get it working?