cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F030K6 device issue

abilashs
Associate II
Posted on June 02, 2014 at 11:22

In this device(STM32F030K6), CLK & DIO signals for SWD are in portA (PA13&PA14). But unknowingly I have changed the default settings of portA(PA13-dio, PA14-clk) and flashed the program. so I want to erase the flash memory through USART after make BOOT0=1 & BOOT1=0(for access system memory).

                    I got to know about Flash loader demonstrator in order to erase my flash data. But it is showing the following error message,

    ''No response from the target, the boot loader cannot be started.''

Though I have made BOOT=1, it is showing the same error. Help me how to solve this issue soon?

       

#stm32-usart-flash-boot-loader
This discussion is locked. Please start a new topic to ask your question.
14 REPLIES 14
Posted on June 02, 2014 at 13:27

How is your USART connected up to the PC? Diagram.

Using a serial terminal app like Real Term, set COM port to 9600 8E1 (8-bit data, EVEN Parity, 1-stop), send hex 0x7F, and observe if you get an 0x79 response.

You should only need to get BOOT0 High to get into the System Loader in most situations.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
abilashs
Associate II
Posted on June 02, 2014 at 13:39

Clive,

In datasheet, they said that PA9 & PA10 pins should be applicable for  reprogram the Flash memory by using USART. But for those 2 pins, USART config are in alternate functions

( default setting is for GPIO). Will it work if i connect Tx Rx to those 2pins.

      

Posted on June 02, 2014 at 16:12

The System Loader software should configure the pins in to a useable fashion, so they won't be in reset conditions at the chip level.

I don't have my STM32F0308-DISCO board to hand right now, but I think that might be workable.

Also from System Loader mode (BOOT0=High, then CPU Reset), should also permit reprogramming or erasure via the SWD interface.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
abilashs
Associate II
Posted on June 03, 2014 at 07:04

Clive,

        Let me tell my hardware connections.

-I have used Max3232 driver (for TTL to RS232 conversion) between controller and PC.

-And also i have made BOOT0 high.

-Then with Flash load demonstrator software, am getting the same error message,

  ''No response from the target, the boot loader cannot be started.''

 Tell me, is it possible to use Hyper terminal for serial communication?

Posted on June 03, 2014 at 16:07

Tell me, is it possible to use Hyper terminal for serial communication?

Well it's not going to be very helpful talking to the System Loader, at least

http://realterm.sourceforge.net/

can send/receive hex data streams.

I've also built my own Windows apps to talk to the System Loader in it's documented protocol.

If your own loader supports X/Y-Modem then a terminal app that supports that would be more useful. But I still like

https://www.clearconnex.com/content/clearterminal

over HyperTerminal

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..