Posted on June 02, 2014 at 13:14Good day friends, Am using STM32F030K6 device for my project. I had met some issue related to SWD, BOOT0/1, Flash and USART things. So i want to know anyone who knows about this device . -welcome.
Posted on June 02, 2014 at 11:22In this device(STM32F030K6), CLK & DIO signals for SWD are in portA (PA13&PA14). But unknowingly I have changed the default settings of portA(PA13-dio, PA14-clk) and flashed the program. so I want to erase the flash m...
Posted on June 03, 2014 at 07:04Clive, Let me tell my hardware connections. -I have used Max3232 driver (for TTL to RS232 conversion) between controller and PC. -And also i have made BOOT0 high. -Then with Flash load demonstrator software, ...
Posted on June 02, 2014 at 13:39Clive, In datasheet, they said that PA9 & PA10 pins should be applicable for reprogram the Flash memory by using USART. But for those 2 pins, USART config are in alternate functions ( default setting is for GPIO). Wi...
Posted on June 02, 2014 at 13:21Hi, In this device(STM32F030K6), CLK & DIO signals for SWD are in portA (PA13&PA14). But unknowingly I have changed the default settings of portA(PA13-dio, PA14-clk) and flashed the program. so debugging wouldn't happ...
Posted on June 02, 2014 at 12:59 But in the datasheet, they have given that BOOT1 is also available. But user can change it only via software. If possible, you pl refer page no 35 in RM0360 (Reference manual)