2020-12-12 7:16 AM
Hi,
I am using stm32f030 to read adc value(truestudio). ADC reads value on an interval of 10 minutes. It is observer that ADC reads value for first 5-6 times,and after that it reads 0v.The readings we get is also different from what is measured on adcpin. what may be the issue??
static void MX_ADC_Init(void)
{
/* USER CODE BEGIN ADC_Init 0 */
/* USER CODE END ADC_Init 0 */
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC_Init 1 */
/* USER CODE END ADC_Init 1 */
/** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/
hadc.Instance = ADC1;
hadc.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc.Init.Resolution = ADC_RESOLUTION_12B;
hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD;
hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc.Init.LowPowerAutoWait = DISABLE;
hadc.Init.LowPowerAutoPowerOff = DISABLE;
hadc.Init.ContinuousConvMode = ENABLE;
hadc.Init.DiscontinuousConvMode = DISABLE;
hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc.Init.DMAContinuousRequests = DISABLE;
hadc.Init.Overrun = ADC_OVR_DATA_PRESERVED;
if (HAL_ADC_Init(&hadc) != HAL_OK)
{
Error_Handler();
}
/** Configure for the selected ADC regular channel to be converted.
*/
sConfig.Channel = ADC_CHANNEL_8;
sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;
sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC_Init 2 */
/* USER CODE END ADC_Init 2 */
}
code for reading value:
while(1){
HAL_ADC_Start(&hadc);
HAL_ADC_PollForConversion(&hadc,100);
u16_adcVal = HAL_ADC_GetValue(&hadc);
HAL_ADC_Stop(&hadc);
}
2020-12-12 9:16 AM
Hello
> sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5
Try to increase the sample time.
Regards
2020-12-13 9:33 AM
Should I disable this or enable:
hadc.Init.ContinuousConvMode
Also sample time to ADC_SAMPLETIME_7CYCLES_5
Along with ADC I also use UART. A GSM module is connected to it. In an interval of 10 min, at 2 minute GSM is made off and at 8th minute GSM is turned on. ADC reads value on every 10th minute. it reads value for first 5 -6 cycle. after that it reads 0.
2020-12-14 1:59 AM
A sample time of 1,5 cycle is very short, for sure.
But it is not a reasonable explanation for the observed effect.
I strongly suspect there is something wrong in your code processing sample date, and not the ADC.
You can try data breakpoints in your debugger - if it supports it.
I.e. a conditional BP at a location, if a variable matches a certain condition (like being 0).
2020-12-14 2:29 AM
"I strongly suspect there is something wrong in your code processing sample date, and not the ADC." Sorry,I didnt get you
2020-12-14 4:26 AM
You probably have a bug elsewhere.
The ADC value gets overwritten during processing.