2017-06-28 4:39 AM
Hi, every one.
I am trying to get data from IrDA SIR mode on STM32F092.
I setup that USART Port 2 is sending IrDA packet and USART Port 1 is receiving ( it similar to loop-back, wired USART2 TX and USART RX )
I can see the irda wave form on USART Port 2 TX Line, but I can't receive any data on USART Port 1.
I hope get any clue what am I missing
Thanks in advance.
Here is our code
IRDA_HandleTypeDef hirda_1;IRDA_HandleTypeDef hirda_2;void HAL_IRDA_MspInit(IRDA_HandleTypeDef *hirda){GPIO_InitTypeDef GPIO_InitStruct;
if(hirda->Instance==USART1) {__HAL_RCC_USART1_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_9|GPIO_PIN_10; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_HIGH; GPIO_InitStruct.Alternate = GPIO_AF1_USART1; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); }if(hirda->Instance==USART2)
{__HAL_RCC_USART2_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_HIGH; GPIO_InitStruct.Alternate = GPIO_AF1_USART2; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); }}
void init_irda(int port ){if ( port == COM_SIR ) {
hirda_1.Instance = USART1;hirda_1.Init.BaudRate = 115200;hirda_1.Init.PowerMode = IRDA_POWERMODE_NORMAL;hirda_1.Init.Parity = IRDA_PARITY_NONE;hirda_1.Init.Prescaler = 1;hirda_1.Init.Mode = IRDA_MODE_TX_RX;hirda_1.Init.WordLength = IRDA_WORDLENGTH_8B;if ( HAL_IRDA_Init(&hirda_1) != HAL_OK ) {Printf('HAL IRDA INIT ERROR ---------\r\n');
}} else if ( port == COM_BT ) {hirda_2.Instance = USART2;
hirda_2.Init.BaudRate = 115200; hirda_2.Init.PowerMode = IRDA_POWERMODE_NORMAL; hirda_2.Init.Parity = IRDA_PARITY_NONE; hirda_2.Init.Prescaler = 1; hirda_2.Init.Mode = IRDA_MODE_TX_RX; hirda_2.Init.WordLength = IRDA_WORDLENGTH_8B;if ( HAL_IRDA_Init(&hirda_2) != HAL_OK ) {
Printf('HAL IRDA INIT ERROR ---------\r\n');
}}}void irda_test()
{ uint8_t Cmd[] = {0x80}; uint8_t ret[10];while(1) {
int retval; memset(ret,0x0,5); Printf('Data Transmit\r\n'); HAL_IRDA_Transmit(&hirda_2,(uint8_t *) Cmd,1,0xFFFF); retval = HAL_IRDA_Receive(&hirda_1,ret,1,1000); if ( retval != HAL_OK ) { Printf('HAL RECEIVE ERROR : %08x\r\n',retval); } else { Printf('Data Received : %02x\r\n',ret[0]); } JOSTimeDly(100);}
}
at Main.c
{
<...>
init_irda(COM_SIR);
init_irda(COM_BT);irda_test();
}
#irda #stm32f02017-06-28 7:26 AM
https://community.st.com/0D50X00009XkXcMSAV
Can we please try not to have duplicative posts on materially the same theme