2014-05-18 9:51 PM
I migrate NXP to ST. Please, could you send all links for work with STM32F0 with coocox.
Links of supportMoviesANEmails of supportDocuments.Thank you. #stm32f02014-05-19 5:58 PM
??
2014-05-19 6:26 PM
??
Did Google, Bing and YouTube break, or something?2014-05-20 11:45 PM
your answer did not help, I need the contacts and links to start working with M0 ST.
2014-05-21 12:00 AM
Start in http://www.st.com/web/catalog/mmc/FM141/SC1169 , pick your mcu family, eg.
http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1574 , pick the particular model, e.g. http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1574/LN7/PF253119 and there click on ''Design Resources''. But if you need this amount of guidance to find the basic documents, you perhaps should consider a different career. JW2014-05-23 7:12 AM
These answers do not help much, the way I see it will be hard to find support via the forum, if the basic is answered imagine the advanced questions.
2014-05-23 8:17 AM
> These answers do not help much,
You basically get what you pay for. I can recommend you consultants at a reasonable rate. JW2014-05-23 9:02 AM
These answers do not help much, the way I see it will be hard to find support via the forum, if the basic is answered imagine the advanced questions.
You are not asking technical questions, you're asking for someone to find things on the internet for you, I have seven year olds that can do that. When you've read through the technical manuals, and tried a few example, and have some questions then, ask those. There isn't email support, if you are a commercial customer contact your local sales office, or FAE's working for your local distributor.2014-05-28 8:37 PM
2014-06-03 11:16 PM