cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F0 Discovery virtual com port of STM32F103

lieven
Associate
Posted on December 05, 2012 at 18:40

STM32F0 Discovery virtual com port of STM32F103

3 REPLIES 3
lieven
Associate
Posted on December 06, 2012 at 00:17

The STM32F103 used for programming  has his serial port connected to the STM32F051. This is probably done with the purpose of using the F103 as VCP to the F051

It would be nice if the F103 could be used at the same time as Virtual comm port and as well as debugging for the F051. 

Can this be done ? 
markr
Associate
Posted on December 14, 2015 at 19:40

I have the same question:

>Can this be done ? 
Posted on December 14, 2015 at 20:39

I have the same question: Can this be done ? 

Two posts from three years ago say no.

The mbed version of the ST-LINK firmware/boards support a VCP function, using a more powerful STM32F103 offering. I'm pretty sure this isn't going to be retrofitted onto older DISCO boards.

Could the firmware be changed to support a VCP, probably, but you'd lose the SWD function.

The mbed firmware is in the NUCLEO boards, use one of those..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..