STM32F0 Discovery Reading ts_cal1 and ts_cal2 from system memory
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-20 1:30 PM
Hi,
I
'm desperate to not achieve my project withthe
internal
temperature
sensor
of
STM32F0
For now I
try to read
the
sensor
factory
calibration
data
stored in the
system memory
by simple
pointer
that way.
(53) uint16_t ts_cal1, ts_cal2; (54) ts_cal1 = *(uint16_t*)(0x1FFFF7B8); (55) ts_cal2 = *(uint16_t*)(0x1FFFF7C2); The KEIL compiler does notappreciate
...
..\main.c(55): error: &sharp77-D: this declaration has no storage class or type specifier ..\main.c(55): error: &sharp28: expression must have a constant valueDo
you have any advice
or
tell me what
I forgot
?Also,
is
that
one
of you
has already managed
to use
the formula in the
datasheet
Temperature
(in
� C) =
{
(
V25-
VSENSE
)/
Avg_Slope
}+
25
? Thanks. #internal-temperature-sensor #internal-temperature-sensorTo give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Labels:
-
ADC
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-20 1:49 PM
It probably doesn't like the way you have the parenthesis
[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Internal%20temperatur%20sensor&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=154]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FInternal%20temperatur%20sensor&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=154Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-20 11:35 PM
By this way. It seems to be OK. No build error. I need to check with the HW now
#define ts_cal1 = *((uint16_t*) 0x1FFFF7B8); #define ts_cal2 = *((uint16_t*) 0x1FFFF7C2); Thank Clive1To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-23 8:38 AM
Internal Temperature sensorwork fine on STM32F0 Discovery. Here the code to save time.
/* Includes ------------------------------------------------------------------*/
#include ''stm32f0xx.h''
#include ''stm32f0_discovery.h''
/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/
#define TS_CAL1 *((uint16_t*) 0x1FFFF7B8) // TS_CAL1 = 1767
#define TS_CAL2 *((uint16_t*) 0x1FFFF7C2) // TS_CAL2 = 1343
#define AVG_SLOPE (float)((TS_CAL1 - TS_CAL2)/0)
/* Private variables ---------------------------------------------------------*/
static
volatile
uint32_t TimingDelay;
uint32_t
clock
=0;
const
uint16_t V25 = 1963;
// V25=1.43V at ref 3.0V
uint16_t VSense;
float
Temp;
/* Private function prototypes -----------------------------------------------*/
void
TimingDelay_Decrement(
void
);
void
Delay(__IO uint32_t nTime);
void
Int_Temp_Sensor_Config(
void
);
float
Get_Int_Temp(
void
);
/* Private functions ---------------------------------------------------------*/
void
Int_Temp_Sensor_Config(
void
)
{
ADC_InitTypeDef ADC_InitStructure;
ADC_StructInit(&ADC_InitStructure);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
ADC_DeInit(ADC1);
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ScanDirection = ADC_ScanDirection_Upward;
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_Init(ADC1, &ADC_InitStructure);
ADC_ChannelConfig(ADC1, ADC_Channel_16, ADC_SampleTime_239_5Cycles);
ADC_TempSensorCmd(ENABLE);
ADC_GetCalibrationFactor(ADC1);
ADC_Cmd(ADC1, ENABLE);
while
(!ADC_GetFlagStatus(ADC1, ADC_FLAG_ADEN));
ADC_StartOfConversion(ADC1);
}
float
Get_Int_Temp(
void
)
{
while
(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET);
VSense = ADC_GetConversionValue(ADC1);
return
(
float
)(((V25 - VSense)/AVG_SLOPE)+25);
}
/**
* @brief Main program.
* @param None
* @retval None
*/
int
main(
void
)
{
/*!< At this stage the microcontroller clock setting is already configured,
this is done through SystemInit() function which is called from startup
file (startup_stm32f0xx.s) before to branch to application main.
To reconfigure the default setting of SystemInit() function, refer to
system_stm32f0xx.c file
*/
RCC_ClocksTypeDef RCC_Clocks;
/* SysTick end of count event each 1ms */
RCC_GetClocksFreq(&RCC_Clocks);
SysTick_Config(RCC_Clocks.HCLK_Frequency / 1000);
/* Initiate Blink Speed variable */
clock
=SystemCoreClock;
/* Configure LED3 and LED4 on STM32F0-Discovery */
STM_EVAL_LEDInit(LED3);
STM_EVAL_LEDInit(LED4);
STM_EVAL_LEDOff(LED3);
STM_EVAL_LEDOff(LED4);
/* Initialize User_Button on STM32F0-Discovery */
STM_EVAL_PBInit(BUTTON_USER, BUTTON_MODE_GPIO);
Int_Temp_Sensor_Config();
while
(1)
{
STM_EVAL_LEDOff(LED4);
Temp = Get_Int_Temp();
Delay(5000);
STM_EVAL_LEDOn(LED4);
Delay(500);
}
/**
* @brief Inserts a delay time.
* @param nTime: specifies the delay time length, in 1 ms.
* @retval None
*/
void
Delay(__IO uint32_t nTime)
{
TimingDelay = nTime;
while
(TimingDelay != 0);
}
/**
* @brief Decrements the TimingDelay variable.
* @param None
* @retval None
*/
void
TimingDelay_Decrement(
void
)
{
if
(TimingDelay != 0x00)
{
TimingDelay--;
}
}
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-23 11:36 AM
A more appropriate cast would be
#define AVG_SLOPE ((float)(TS_CAL1 - TS_CAL2)/0)
Up vote any posts that you find helpful, it shows what's working..