cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F0/3xx TIM16/17 registers/pins compared to STM32L15xVEY WLCSP104

louisbirk
Associate
Posted on September 22, 2016 at 02:57

Looking at AN4099 app note its not clear that the STM32L151VEY has the same capabilities/software support as the STM32F0xx in terms of setting up TIM16/17 for GPIO (PB9) for infrared txcr. Is it possible to configure the former to perform the same as the latter for ir xmit/rec ? 

#stm32l151xvey
1 REPLY 1
Amel NASRI
ST Employee
Posted on September 22, 2016 at 14:13

Hi birk.louis,

Only STM32F0 and STM32F3 are supported by AN4099.

Referring to

http://www.st.com/content/ccc/resource/technical/document/datasheet/group1/a7/13/6a/ce/1f/f3/40/c1/DM00098321/files/DM00098321.pdf/jcr:content/translations/en.DM00098321.pdf

and

http://www.st.com/content/ccc/resource/technical/document/reference_manual/cc/f9/93/b2/f0/82/42/57/CD00240193.pdf/files/CD00240193.pdf/jcr:content/translations/en.CD00240193.pdf

, there is no infrared interface in STM32L151VEY.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.