2016-09-21 05:57 PM
Looking at AN4099 app note its not clear that the STM32L151VEY has the same capabilities/software support as the STM32F0xx in terms of setting up TIM16/17 for GPIO (PB9) for infrared txcr. Is it possible to configure the former to perform the same as the latter for ir xmit/rec ?
#stm32l151xvey2016-09-22 05:13 AM
Hi birk.louis,
Only STM32F0 and STM32F3 are supported by AN4099.Referring to and , there is no infrared interface in STM32L151VEY.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.