2018-01-24 12:59 PM
Hi,
A question mostly aimed at ST - do you plan to release USB LL drivers?
At least for F1 & L4 USB LL drivers are not generated.
Bogdan
2018-01-24 03:57 PM
The
contains this note (Section 3 - Overview):LL APIs are not provided for peripherals where optimized access is not a key feature, or those requiring heavy software configuration and/or complex upper-level stack (such as FSMC, USB or SDMMC).
So maybe there are technical limitations to having the LL API for USB?
2018-01-24 04:33 PM
Yes - I really wouldn't have thought that 'LL' was appropriate to stuff like USB.
2018-01-24 09:53 PM
Yes, make sense. I just finished the development of a USB bootloader where I use mostly LL drivers, and the only one consuming most flash is the USB. That's why I asked this question.