2016-07-06 07:22 AM
Running the install SetupSTM32CubeMX-4.15.1.linux
crashes. OS: Ubuntu 16.04LTS 64 Bitjava version:java -versionopenjdk version ''9-internal''OpenJDK Runtime Environment (build 9-internal+0-2016-04-14-195246.buildd.src)OpenJDK 64-Bit Server VM (build 9-internal+0-2016-04-14-195246.buildd.src, mixed mode)Attached is crash logSolved! Go to Solution.
2017-05-18 06:04 PM
Yes, it does. Thank you issue resolved.
2016-07-13 06:07 AM
Hi michals.tim,
I have an issue to open your crash log.Could you please reattach it? -Syrine-2016-07-14 08:09 AM
I have a similar problem with the same operating system. When I try:
cd to directory where the file SetupSTM32CubeMX-4.15.1.linux is located $ sudo ./SetupSTM32CubeMX-4.15.1.linux The installer runs but always generates the following message: sudo: unable to execute ./SetupSTM32CubeMX-4.15.1.linux: No such file or directory Tried the default openjdk as well as oracle java. The last version of of the installer that worked was SetupSTM32CubeMX-4.13.0.linux with oracle java. Later versions do not. Hopefully one day this problem will resolved. Regards ...2016-07-14 09:22 AM
2016-07-21 03:11 AM
Dear all,
We do not reproduce your issue.
Please note STM32CubeMX on Linux is a 32 bit application. Do you confirm that you have 32 bit compliant packages installed on your Linux 64 bit?
The tool also requires: java 1.7.0_45 or later.
Best regards
2017-02-02 03:05 AM
Hello All,
CubeMX-4.19 with oracle java version 1.8.0_121, on Ubuntu 64 bits has been tested.
IT works well.
I was able to install, launch and creates a project.
Has this thread was long ago, I guess everything has been fixed since.
Kind regards
Sirma
2017-05-18 06:04 PM
Yes, it does. Thank you issue resolved.