2014-05-18 2:28 AM
Hello,
when generating a project with STM32CubeMX for a STM32F4discovery board, the PD12 to PD15 pins are configured output (for the LEDs) automatically. But the project is not entirely configured. I had to manually set ''output push pull'' under configuration -> GPIO. It's quite confusing because the project is only partialy configured.@ST : you could ''fix'' that in next version.2014-05-20 7:34 AM
Hi,
This limitation is already detected, and will be fixed in STM32CubeMX V4.3With regards.