cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX Stm32F4discovery configuration

atsju2
Associate II
Posted on May 18, 2014 at 11:28

Hello,

when generating a project with STM32CubeMX for a STM32F4discovery board, the PD12 to PD15 pins are configured output (for the LEDs) automatically. But the project is not entirely configured. I had to manually set ''output push pull'' under configuration -> GPIO. It's quite confusing because the project is only partialy configured.

@ST : you could ''fix'' that in next version.
1 REPLY 1
Posted on May 20, 2014 at 16:34

Hi,

This limitation is already detected, and will be fixed in STM32CubeMX V4.3

With regards.