cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX Problem during Download (not yet available)

Posted on October 26, 2016 at 09:36

Hi,

if I want to install a new Library, always the following message appears:

''The Files have problem during Download:

....zip (Not yet available)

For unavailable files, you can load them manually with the ''From Local'' button.''

This happens with any package I selected. I use the newest version 4.17.0 from STM32CubeMX.

I also tried to install it from local, but this also won�t work.

Thank you for any help.

#download #available
4 REPLIES 4
slimen
Senior
Posted on October 26, 2016 at 11:39

Hello corMat,

 I have successfully download and install some packages! Maybe in your case a server is down for few minutes. So, you can try again. 

Also, check if you have space enough in your disk.

Which package do you need ? May be I can send you the needed package to find a way out of that situation.

Regards

Posted on October 26, 2016 at 11:59

Hi forumstm32,

I tried it now over hours, but always with the same result.

I have enough free space (260GB), so this isn´t the problem.

I need the package for Family STM32L4 v1.5.2 (stm32cube_fw_l4_v150.zip)

Regards

slimen
Senior
Posted on October 26, 2016 at 12:23

Hi,

Here is the

https://drive.google.com/file/d/0B-KpPbIrv-E0MmxHSURqQzdZUFk/view?usp=sharing

 link. Hope this help you.

About your issue, may be you should delete the cookies, un-install CubeMx/library, then  try again the install.  

Regards

Posted on October 26, 2016 at 13:04

Hi,

thank you a lot for the package.

Now it seems to work with the local installation.

Regards