cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX + HAL + LWIP(RAW API) + DP84848 Don't work

tome
Associate II
Posted on July 02, 2017 at 14:08

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on July 05, 2017 at 20:05

Hi Amel,

Sorry for the late answer, and thanks for your attention to this issue. I was out of office and answering from smartphone is not casual.

1. Yes, the project is on the stm32f107.

2. It write something like 4.18.0, STM32Cube FW_F1 v.1.4.0 and as I understand it use old version lib's (it downloads DB.4.0.180.tar.bz2)

3. Yes. Then I deinstall the Cube and install it agin. It didn't help me.

Usually, I fixed the issue and project is working now.

I replaced one variable in function void TCP_server_init(void)

err = tcp_bind(pcb, addr, TCP_PORT);

with the 

err = tcp_bind(pcb, IP_ADDR_ANY, TCP_PORT);

So, I think for now we can close this topic.

View solution in original post

2 REPLIES 2
Amel NASRI
ST Employee
Posted on July 03, 2017 at 16:46

Hi

Kirichok.Sergey

‌,

Could you please precise the following:

  • used device is STM32F107, right?
  • what 'old' CubeMX version were you using?
  • you updated to the version .21 of CubeMX and then problem started to be faced,right?

Then it is interesting to share the 'old working project' before update. Is it available somewhere?

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on July 05, 2017 at 20:05

Hi Amel,

Sorry for the late answer, and thanks for your attention to this issue. I was out of office and answering from smartphone is not casual.

1. Yes, the project is on the stm32f107.

2. It write something like 4.18.0, STM32Cube FW_F1 v.1.4.0 and as I understand it use old version lib's (it downloads DB.4.0.180.tar.bz2)

3. Yes. Then I deinstall the Cube and install it agin. It didn't help me.

Usually, I fixed the issue and project is working now.

I replaced one variable in function void TCP_server_init(void)

err = tcp_bind(pcb, addr, TCP_PORT);

with the 

err = tcp_bind(pcb, IP_ADDR_ANY, TCP_PORT);

So, I think for now we can close this topic.