2017-10-18 11:33 PM
Hi all
I'm new to stm32 and have troubles to install the CubeMX Standalone and Eclipse Plugin.
I've downloaded the archive fro st.com, unarchive made the installer executable but the installer dosn't start.
When i tried to start from command line
[tino@archlinux en.stm32cubemx]$ ./SetupSTM32CubeMX-4.22.1.linux
bash: ./SetupSTM32CubeMX-4.22.1.linux: No such file or directoryI've triy also as Eclipse plugin, Its running but after some time the eclipse window starts flicker.
java version '1.8.0_152'
Java(TM) SE Runtime Environment (build 1.8.0_152-b16) Java HotSpot(TM) 64-Bit Server VM (build 25.152-b16, mixed mode)2017-10-19 12:46 AM
Hello,
Make sure to follow instructions in the STM32CubeMX User Manual
.Please note that STM32CubeMX on Linux is a 32-bit application,
some versions of Linux 64-bit distributions require to install 32-bit compliant packages such as ia32-libs.
Do you confirm that you have 32-bit compliant packages installed on your Linux 64-bit?
Kind Regards
Imen
2017-11-06 3:21 PM
,
,
I had the same problem on 64-bit Ubuntu 16.04:
bash: ./SetupSTM32CubeMX-4.23.0.linux: No such file or directory
This askubuntu post solved it for me:
https://askubuntu.com/questions/454253/how-to-run-32-bit-app-in-ubuntu-64-bit/454254 ♯ 454254
,2017-12-03 1:09 PM
for my Linux Fedora 26 64 bit need:
1.
sudo dnf install glibc.i686
2../SetupSTM32CubeMX-4.23.0.linux