2017-11-30 08:32 AM
I am having the same issue with STM32CubeMX 4.23.0 that I had with the previous version. Having upgraded to Ubuntu 17.10 I can't select the ok button to set my Project settings in CubeMX. Any ideas on how I can select the ok button, key combinations etc ? I have tried resolution changes different ways to scroll but nothing works. Could the designers of Cubemx please make the project settings dialog of future versions resizable ?
2017-12-18 09:48 AM
Hello,
Have you used the Zoom feature (available from the toolbar) ? or tried <CTRL> + Mousewheel to Zoom in or out?
Best Regards
Imen
2017-12-18 11:38 AM
<CTRL> + Mousewheel to Zoom in or out
Doesn't do anything in the project settings dialog and zooming in the
project window has no effect on the project settings dialog.
>Have you used the Zoom feature (available from the toolbar) ?
Isn't available in the Project settings dialog.
Thanks for trying any other ideas welcome.
Regards,
David