cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 4.23.0 project settings dialog, can't select OK in Ubuntu 17.10

David Fisher
Associate II
Posted on November 30, 2017 at 17:32

I am having the same issue with STM32CubeMX 4.23.0 that I had with the previous version. Having upgraded to Ubuntu 17.10 I can't select the ok button to set my Project settings in CubeMX. Any ideas on how I can select the ok button, key combinations etc ? I have tried resolution changes different ways to scroll but nothing works. Could the designers of Cubemx please make the project settings dialog of future versions resizable ?

2 REPLIES 2
Imen.D
ST Employee
Posted on December 18, 2017 at 18:48

Hello,

Have you used the Zoom feature (available from the toolbar) ? or tried <CTRL> + Mousewheel to Zoom in or out?

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on December 18, 2017 at 19:38

<CTRL> + Mousewheel to Zoom in or out

Doesn't do anything in the project settings dialog and zooming in the

project window has no effect on the project settings dialog.

>Have you used the Zoom feature (available from the toolbar) ?

Isn't available in the Project settings dialog.

Thanks for trying any other ideas welcome.

Regards,

David