cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeL4

ax0018
Associate III
Posted on October 25, 2017 at 03:11

STM32CubeL4 1.10 is listed on the website, but version 1.9.0 is inside the .zip file when downloaded.

11 REPLIES 11
Posted on October 25, 2017 at 04:57

The directory name, or some of the specific files?

\STM32Cube_FW_L4_V1.10.0\Drivers\BSP\STM32L4xx_Nucleo_32\stm32l4xx_nucleo_32.c

https://drive.google.com/open?id=0B7OY5pub_GfIZVVxcGhJVGR4SnM

 

1.9.0 was listed on the website earlier, while 1.10.0 was available inside CubeMX, mind that it is a 1.7GB download

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on October 25, 2017 at 04:59

Assuming you downloaded this 

http://www.st.com/en/embedded-software/stm32cubel4.html

 and it wasn't as advertised...

Wonder if they use a caching provider, or someone has Squid downstream. A smarter strategy might be to give each release a unique filename...

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on October 25, 2017 at 14:27

Can confirm that it was pulling V1.9.0 last night at the time of the previous post.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Imen.D
ST Employee
Posted on October 25, 2017 at 17:47

Hello,

This problem is fixed and I have successfully download the package.

Could you please check from your side and let me known ? 

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on October 25, 2017 at 20:35

v1.9.0 - 709MB, vs v1.10.0 - 1.88GB

Extra space(~`1.1GB)  mostly consumed by the project examples for STM32L4R9I-Discovery and STM32L4R9I-EVAL boards. This must be really cool board:) Have you ever seen it?

Posted on October 25, 2017 at 19:47

Pulling 1.8GB V1.10.0 in North America now.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on October 25, 2017 at 20:44

This is the new

https://community.st.com/0D50X00009XkXG8SAN

, to be announced.

JW

Posted on October 25, 2017 at 22:26

Thank you. Solved.

Posted on October 25, 2017 at 22:44

>>

This must be really cool board:)

Should be able to make me breakfast...

The current crop of L4 run at 120 MHz, so not a long drive to get there, 640 KB RAM, 2MB FLASH

http://www.keil.com/dd2/stmicroelectronics/stm32l4r9aiix/

 

Gerbers for the EVAL

https://keilpack.azureedge.net/content/Keil.STM32L4xx_DFP.2.0.0/MDK/Boards/ST/STM32L4R9I-EVAL/Documentation/stm32l4r9i-eval_gerber.zip

 
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..