2017-10-24 06:11 PM
STM32CubeL4 1.10 is listed on the website, but version 1.9.0 is inside the .zip file when downloaded.
2017-10-24 07:57 PM
The directory name, or some of the specific files?
\STM32Cube_FW_L4_V1.10.0\Drivers\BSP\STM32L4xx_Nucleo_32\stm32l4xx_nucleo_32.c
https://drive.google.com/open?id=0B7OY5pub_GfIZVVxcGhJVGR4SnM
1.9.0 was listed on the website earlier, while 1.10.0 was available inside CubeMX, mind that it is a 1.7GB download
2017-10-24 09:59 PM
Assuming you downloaded this
http://www.st.com/en/embedded-software/stm32cubel4.html
and it wasn't as advertised...Wonder if they use a caching provider, or someone has Squid downstream. A smarter strategy might be to give each release a unique filename...
2017-10-25 07:27 AM
Can confirm that it was pulling V1.9.0 last night at the time of the previous post.
2017-10-25 08:47 AM
Hello,
This problem is fixed and I have successfully download the package.
Could you please check from your side and let me known ?
Best Regards
Imen
2017-10-25 11:35 AM
v1.9.0 - 709MB, vs v1.10.0 - 1.88GB
Extra space(~`1.1GB) mostly consumed by the project examples for STM32L4R9I-Discovery and STM32L4R9I-EVAL boards. This must be really cool board:) Have you ever seen it?
2017-10-25 12:47 PM
Pulling 1.8GB V1.10.0 in North America now.
2017-10-25 01:44 PM
This is the new
https://community.st.com/0D50X00009XkXG8SAN
, to be announced.JW
2017-10-25 03:26 PM
Thank you. Solved.
2017-10-25 03:44 PM
>>
This must be really cool board:)
Should be able to make me breakfast...
The current crop of L4 run at 120 MHz, so not a long drive to get there, 640 KB RAM, 2MB FLASH
http://www.keil.com/dd2/stmicroelectronics/stm32l4r9aiix/
Gerbers for the EVAL