2018-07-05 7:31 AM
How am I importing the sample projects for STM32L476VGT6 from the STM32CUBEMX Repository 'stm32cube_fw_l4_v1120.zip' into the 'System Workbench for STM32' (eclipse STM32 compiler)?
I purchased the STM32L476 Discovery board.
Please post steps of how to import all or individual sample project into the
'
System Workbench for STM32 /AC6 tools'
Thank you
#stm32l476 #ac6-system-workbench-for-stm322018-07-05 7:40 AM
Open the project in your tool chain
STM32Cube_FW_L4_V1.12.0\Projects\32L476GDISCOVERY\Examples\CRC\CRC_UserDefinedPolynomial\SW4STM32\STM32L476G-Discovery
2018-07-05 7:50 AM
Hello
swctrlhw
,As said Clive, you can open an existing project under STM32CubeL4 package with SW4STM32.
Have a look to the
User manual Getting started with STM32CubeL4 and follow the steps in the &39Running the first example&39 section, which explains how to run a first example within STM32CubeL4 using SW4STM32.With Regards,
Imen
2018-07-05 10:45 AM
Hello all,
Thank you. It is working.
On Thu, Jul 5, 2018 at 10:50 AM Imen D <st-microelectronics@jiveon.com>