STM32Cube_FW_H7_V1.2.0 Bugs - NUCLEO HSE_VALUE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-15 9:29 AM
STM32Cube_FW_H7_V1.2.0\Projects\STM32H743ZI-Nucleo\Applications\FatFS\FatFS_uSD_Standalone\Inc\stm32h7xx_hal_conf.h
\STM32Cube_FW_H7_V1.2.0\Projects\STM32H743ZI-Nucleo\Applications\LwIP\LwIP_HTTP_Server_Netconn_RTOS\Inc\stm32h7xx_hal_conf.h
Nucleo uses 8 MHz HSE in BYPASS mode, the wrong HSE_VALUE breaks USART, rate computations, etc
/**
* @brief Adjust the value of External High Speed oscillator (HSE) used in your application. * This value is used by the RCC HAL module to compute the system frequency * (when HSE is used as system clock source, directly or through the PLL). */#if !defined (HSE_VALUE)#define HSE_VALUE ((uint32_t)25000000) /*!< Value of the External oscillator in Hz */#endif /* HSE_VALUE */Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-15 12:35 PM
CubeMX also used or still use(s) wrong default HSE freq on some nucleo boards.
Reported this here
https://community.st.com/0D50X00009XkYXhSAN
Took me awhile to get a 767 project last last night because it still wasn't fixed in 4.23!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-15 1:59 PM
Banged my head on this working on the H743ZI-NUCLEO this morning, had been working via the VCP/USART3 and then started porting the SDMMC project. The symptom looked like an issue with HSE_VALUE so the first thing I checked. Likely other errors, pulled these two with a quick scan, but does highlight the need for more rigour in the releases here.
Didn't manage to get the SDMMC to work on the board, and did strip out the level converter stuff. Have pivoted back to the F767ZI-NUCLEO to get that working with the MicroSD socket to sanity check things.
The STM32H743I-EVAL arrived so will bang on that too.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-15 3:02 PM
LOL! i did almost the exact same thing last night.
Got my FatFS/SDIO working disco-411, and decide to move to the NUC-767 board before adding FreeRTOS in the fray.
Couldn't get it working for about 2hrs! and sdio was clocking was off what i expected, so i added MCO and figured the whole clk setup was wrong from CubeMX.
Then i found the 16MHz HSE input freq in cube!
But, what's worse is this my second time! Forget i reported it, until you posted! LOL
FYI, Waveshare SD breakout is working fine on 1bit (haven't bothered with 4bit yet)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-15 3:30 PM
I'd picked up several of the ViewTool version
https://www.ebay.com/itm/1pcs-NEW-Micro-SD-Card-Module-Slot-Socket-Reader/272798769771
Nucleo F767ZI
Core=216000000, 216 MHzCPUID 411FC270 DEVID 451Cortex M7 r1p0STM32F76xxx or F77xxxC0000000 FFFFFFF8 0000000010110221 12000011 00000040FPU-D Single-precision and Double-precisionAPB1=54000000APB2=108000000FatFs Testing (68300)SystemCoreClock: 216000000Mounting FatFsFAT32 30.4 GB total drive space 30.3 GB available 100.3 MB used---- 113 /DIR.TXT---- 175 /LOG.TXTD--- 0 /RINEX---- 32768000 /SPEEDTST.BIND--- 0 /BASE_301---- 2494 /RINEX.INI32768000 Bytes, 524170395 Cycles 13.50 MBps Read (FatFs)32768000 Bytes, 524151419 Cycles 13.50 MBps Read (FatFs)4864 ms 13.47 MBps200005A0 512
CrcFile Size:32768000 BufferSize:512 32768000 CRC32:65744B39 PKZIP:9A8BB4C6 SPEEDTST.BIN200005A0 1024CrcFile Size:32768000 BufferSize:1024 32768000 CRC32:65744B39 PKZIP:9A8BB4C6 SPEEDTST.BIN200005A0 4096CrcFile Size:32768000 BufferSize:4096 32768000 CRC32:65744B39 PKZIP:9A8BB4C6 SPEEDTST.BIN200005A0 20480CrcFile Size:32768000 BufferSize:20480 32768000 CRC32:65744B39 PKZIP:9A8BB4C6 SPEEDTST.BIN200005A0 32768CrcFile Size:32768000 BufferSize:32768 32768000 CRC32:65744B39 PKZIP:9A8BB4C6 SPEEDTST.BIN200005A0 40960CrcFile Size:32768000 BufferSize:40960 32768000 CRC32:65744B39 PKZIP:9A8BB4C6 SPEEDTST.BIN200005A0 65536CrcFile Size:32768000 BufferSize:65536 32768000 CRC32:65744B39 PKZIP:9A8BB4C6 SPEEDTST.BINDone..Infinite loop...Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-23 9:21 AM
Hi Clive,
You have to select init Peripherals when loading the board to get the right default configuration
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-23 1:21 PM
>>You have to select init Peripherals when loading the board to get the right default configuration
Sorry, I don't understand the response. These are examples in the HAL code trees, supposedly ready to build and tested, not output from CubeMX...
The code settings for HSE_VALUE is demonstrably wrong, and causes the clocking in the system to be incorrectly computed.
Up vote any posts that you find helpful, it shows what's working..