cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CUBE and USB framework

thierry1
Associate II
Posted on April 23, 2014 at 15:46

Has the USB framework supplied with STM32CubeF4 been completely rewritten or is it  the USB-Host-Device_Lib_V2.1.0?

2 REPLIES 2
rigomate2
Associate III
Posted on April 24, 2014 at 09:48

Why not do a compare of them with any common compare tool?

chen
Associate II
Posted on April 24, 2014 at 11:38

I do not think it is as simple as doing a compare.

1. (from what I understand) The Cube tool generates the code for the specified processor and environment (OS, IDE etc)

2. Since one generates code for specific processors and the other has to cater for a number of processors - one will contain compiler directive and the other will not.

2. Naming conventions are different between the 2