cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CO11 DELAYS NOT WORKING

meena
Associate III

 

if(Mains>0.1) { if((Mains<1) &&(Vbat>0.9)) { TIM1->CCR4=TIM1->ARR; HAL_TIM_PWM_Start(&htim1,TIM_CHANNEL_4); Set_LED(0); Batt_Chrge(0); HAL_Delay(1000); } else { TIM1->CCR4=0; HAL_TIM_PWM_Start(&htim1,TIM_CHANNEL_4); Batt_Chrge(0); } if((Mains<0.1)&&(HAL_GPIO_ReadPin(GPIOA,GPIO_PIN_6)==GPIO_PIN_SET)) { TIM1->CCR4=TIM1->ARR/2; HAL_TIM_PWM_Start(&htim1,TIM_CHANNEL_4); Batt_Chrge(0); } else if((Mains<0.1)&&(HAL_GPIO_ReadPin(GPIOA,GPIO_PIN_6)==GPIO_PIN_RESET)) { TIM1->CCR4=TIM1->ARR; HAL_TIM_PWM_Start(&htim1,TIM_CHANNEL_4); Batt_Chrge(0); } } /*REST OF MY CODE*/ if((Mains<0.1)&& (TIM1->CCR4 == 0)) { count++; if(count>=50) { Enter_sleep(); } }
View more

hi can anyone please let me what is wrong ,these code should be worked only detecting the mains as after Mains>0.1 if interruptions occur it should start again only after mains>0.1.I have also configured SYSTICK but I am not  sure why my delay is not working .

 

2 REPLIES 2
TDK
Super User

What isn't working about the code in particular? Perhaps break it into smaller sections and try those. If delay isn't working, move that logic into a simpler block.

Consider debugging and stepping through the code to find out what isn't working as expected and why.

If you feel a post has answered your question, please click "Accept as Solution".

Lacking a lot of context here.

Are you doing this in an interrupt/callback ? Going to be priority/preemption issues there if relying on SysTick, etc, to advance the software tick counter.

You'd need to differ execution using other methods, so you can leave the callback immediately.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..