cancel
Showing results for 
Search instead for 
Did you mean: 

STM32C011F6U7 MCU schematic Reset and programming tool

gavin3
Associate II

Hi Guys,

I will use STM32C011F6U7 did my devices development, but I can not certain that the schematic is correct or not, is right for NRST part? same time I want to know what tools should I used to download FW to units, 5 pins J-LINK or others 4 pins tool? any comments?

gavin3_0-1712050121861.png

gavin3_2-1712050147176.png

 

2 REPLIES 2
STTwo-32
ST Employee

Hello @gavin3 

I suggest you refer to the AN5673 to have tips on design using the STM32C0.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Simon.T
ST Employee

Hello @gavin3 ,

 

As @STTwo-32  said you can follow the AN5673 hardware getting started, or you can also take the NUCLEO-C031C6 schematic as reference. 

Also an internal pull up is already present inside the NRST pin, so I recommend you to remove the external pull up.

 

Best regards,

 

Simon